HatchFillSettingsBuilderAnnotationTypes Enumeration

NXOpen.Annotations.HatchFillSettingsBuilder.AnnotationTypes is an alias for NXOpen.Annotations.HatchFillSettingsBuilderAnnotationTypes

class NXOpen.Annotations.HatchFillSettingsBuilderAnnotationTypes

Bases: object

the valid types of hatch objects

Enum Members

Enum Member Enum Member Description
Crosshatch
Crosshatch
AreaFill
Area Fill
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.