GeometricCharacteristic Enumeration¶
-
class
NXOpen.Annotations.
GeometricCharacteristic
¶ Bases:
object
Specifies the geometric characteristic for an FCF Enum Members
Enum Member Enum Member Description Straightness Specifies straightnesss characteristicsFlatness Specifies flatness characteristicsCircular Specifies cirular characteristicsCylindrical Specifies cylindrical characteristicsLineProfile Specifies line profile characteristicsSurfaceProfile Specifies surface profile characteristicsAngular Specifies angular characteristicsPerpendicular Specifies perpendicular characteristicsParallel Specifies parallel characteristicsPosition Specifies position characteristicsConcentric Specifies concentric characteristicsSymmetric Specifies symmetric characteristicsCircularRunout Specifies cirular runout characteristicsTotalRunout Specifies total runout characteristicsLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-