GeodesicDimensionBuilder Class¶
-
class
NXOpen.Annotations.
GeodesicDimensionBuilder
¶ Bases:
NXOpen.Builder
Represents a
Annotations.Dimension
builderTo create a new instance of this class, use
NXOpen.Annotations.DimensionCollection.CreateGeodesicDimensionBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Driving | Returns the driving value builder, which manages driving dimension values |
Measurement | Returns the measurement |
MeasurementPoint | Returns the measurement point |
Origin | Returns the origin |
OriginCurve | Returns the curves or edges to dimension from |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Driving¶
-
GeodesicDimensionBuilder.
Driving
¶ Returns the driving value builder, which manages driving dimension values
-------------------------------------
Getter Method
Signature
Driving()
Returns: Return type: NXOpen.Annotations.DrivingValueBuilder
New in version NX10.0.0.
License requirements: None.
Measurement¶
-
GeodesicDimensionBuilder.
Measurement
¶ Returns the measurement
-------------------------------------
Getter Method
Signature
Measurement()
Returns: Return type: NXOpen.Annotations.DimensionMeasurementBuilder
New in version NX10.0.0.
License requirements: None.
MeasurementPoint¶
-
GeodesicDimensionBuilder.
MeasurementPoint
¶ Returns the measurement point
-------------------------------------
Getter Method
Signature
MeasurementPoint()
Returns: Return type: NXOpen.SelectPoint
New in version NX10.0.0.
License requirements: None.
Origin¶
-
GeodesicDimensionBuilder.
Origin
¶ Returns the origin
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX10.0.0.
License requirements: None.
OriginCurve¶
-
GeodesicDimensionBuilder.
OriginCurve
¶ Returns the curves or edges to dimension from
-------------------------------------
Getter Method
Signature
OriginCurve()
Returns: Return type: NXOpen.SelectEdge
New in version NX10.0.0.
License requirements: None.
Style¶
-
GeodesicDimensionBuilder.
Style
¶ Returns the style
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
GeodesicDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.