ForeshorteningSymbolSettingsBuilder Class¶
-
class
NXOpen.Annotations.
ForeshorteningSymbolSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.ForeshorteningSymbolSettingsBuilder
builderNew in version NX10.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns or sets the foreshortening symbol angle |
ForeshorteningSymbolMethodType | Returns or sets the foreshortening symbol method |
ForeshorteningSymbolType | Returns or sets the foreshortening symbol type |
Height | Returns or sets the foreshortening symbol height |
Tag | Returns the Tag for this object. |
Width | Returns or sets the foreshortening symbol width |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ForeshorteningSymbolSettingsBuilderMethodType Enumeration | Represents foreshortening symbol method type |
ForeshorteningSymbolSettingsBuilderSymbolType Enumeration | Represents foreshortening symbol type |
Property Detail¶
Angle¶
-
ForeshorteningSymbolSettingsBuilder.
Angle
¶ Returns or sets the foreshortening symbol angle
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Angle(foreshorteningSymbolAngle)
Parameters: foreshorteningSymbolAngle (float) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
ForeshorteningSymbolMethodType¶
-
ForeshorteningSymbolSettingsBuilder.
ForeshorteningSymbolMethodType
¶ Returns or sets the foreshortening symbol method
-------------------------------------
Getter Method
Signature
ForeshorteningSymbolMethodType()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolSettingsBuilderMethodType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForeshorteningSymbolMethodType(foreshorteningSymbolMethod)
Parameters: foreshorteningSymbolMethod ( NXOpen.Annotations.ForeshorteningSymbolSettingsBuilderMethodType
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
ForeshorteningSymbolType¶
-
ForeshorteningSymbolSettingsBuilder.
ForeshorteningSymbolType
¶ Returns or sets the foreshortening symbol type
-------------------------------------
Getter Method
Signature
ForeshorteningSymbolType()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolSettingsBuilderSymbolType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForeshorteningSymbolType(foreshorteningSymbolType)
Parameters: foreshorteningSymbolType ( NXOpen.Annotations.ForeshorteningSymbolSettingsBuilderSymbolType
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Height¶
-
ForeshorteningSymbolSettingsBuilder.
Height
¶ Returns or sets the foreshortening symbol height
-------------------------------------
Getter Method
Signature
Height()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Height(foreshorteningSymbolHeight)
Parameters: foreshorteningSymbolHeight (float) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Width¶
-
ForeshorteningSymbolSettingsBuilder.
Width
¶ Returns or sets the foreshortening symbol width
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Width(foreshorteningSymbolWidth)
Parameters: foreshorteningSymbolWidth (float) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
ForeshorteningSymbolSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.