FlipOption Enumeration

class NXOpen.Annotations.FlipOption

Bases: object

Specifies the custom symbol flip option.

This option is only available when editing. This option is unavailable for symbols with leaders. Enum Members

line taken through its anchor point “
“Vertical”, ” Flips a symbol vertically about a horizontal
line taken through its anchor point “
“Last”, ” Last enum value. Should not be used. “
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.