FeatureControlFrameDataBuilderToleranceMaterialModifier Enumeration¶
NXOpen.Annotations.FeatureControlFrameDataBuilder.ToleranceMaterialModifier is an alias for NXOpen.Annotations.FeatureControlFrameDataBuilderToleranceMaterialModifier
-
class
NXOpen.Annotations.
FeatureControlFrameDataBuilderToleranceMaterialModifier
¶ Bases:
object
Specifies the tolerance material modifier condition
Enum Members
Enum Member Enum Member Description NotSet no material modifierLeastMaterialCondition least material conditionMaximumMaterialCondition maximum material conditionRegardlessOfFeatureSize regardless of feature size condition-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-