FeatureControlFrameBuilderFcfCharacteristic Enumeration

NXOpen.Annotations.FeatureControlFrameBuilder.FcfCharacteristic is an alias for NXOpen.Annotations.FeatureControlFrameBuilderFcfCharacteristic

class NXOpen.Annotations.FeatureControlFrameBuilderFcfCharacteristic

Bases: object

Specifies the characteristitic of the feature control frame

Enum Members

Enum Member Enum Member Description
Straightness
straightness
Flatness
flatness
Circularity
circularity
Cylindricity
cylindricity
ProfileOfALine
profile of a line
ProfileOfASurface
profile of a sufrace
Angularity
angularity
Perpendicularity
perpendicularity
Parallelism
parallelism
Position
position
Concentricity
concentricity
Symmetry
symmetry
CircularRunout
circular runout
TotalRunout
total runout
AxisIntersection
axis intersection
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.