EditSymbolDisplayBuilderWidthTypes Enumeration¶
NXOpen.Annotations.EditSymbolDisplayBuilder.WidthTypes is an alias for NXOpen.Annotations.EditSymbolDisplayBuilderWidthTypes
-
class
NXOpen.Annotations.
EditSymbolDisplayBuilderWidthTypes
¶ Bases:
object
The Enum represent width types
NXOpen.Annotations.EditSymbolDisplayBuilder.WidthTypes()
andNXOpen.Annotations.EditSymbolDisplayBuilder.WidthTypes()
will set this width type at builder side and will be used to apply the same on the selected contents after commitEnum Members
.
- . csv-table::
header: “Enum Member”, “Enum Member Description” “Thin”, ” Thin ” “Normal”, ” Normal ” “Thick”, ” Thick ” “ThicknessOne”, ” Width One ” “ThicknessTwo”, ” Width Two ” “ThicknessThree”, ” Width Three ” “ThicknessFour”, ” Width Four ” “ThicknessFive”, ” Width Five ” “ThicknessSix”, ” Width Six ” “ThicknessSeven”, ” Width Seven ” “ThicknessEight”, ” Width Eight ” “ThicknessNine”, ” Width Nine “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.