EditSymbolDisplayBuilderFontTypes Enumeration¶
NXOpen.Annotations.EditSymbolDisplayBuilder.FontTypes is an alias for NXOpen.Annotations.EditSymbolDisplayBuilderFontTypes
-
class
NXOpen.Annotations.
EditSymbolDisplayBuilderFontTypes
¶ Bases:
object
The Enum represent font types.
NXOpen.Annotations.EditSymbolDisplayBuilder.FontTypes()
andNXOpen.Annotations.EditSymbolDisplayBuilder.FontTypes()
will set this font type at builder side and will be used to apply the same on the selected contents after commitEnum Members
Enum Member Enum Member Description Solid Solid typeDashed Dashed TypePhantom Phantom TypeCenterline CenterlineDotted Dotted TypeLongDashed Long DashDottedDashed Dotted Dash-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-