DrawingFormatTitleBuilder Class¶
-
class
NXOpen.Annotations.
DrawingFormatTitleBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.DrawingFormatTitleBuilder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Automatic | Returns or sets the flag that determines whether or not the title block updates automatically whenever a change occurs to a referenced object in the model |
Tag | Returns the Tag for this object. |
TitleBlockAlignmentPosition | Returns or sets the option that specifies how the title block aligns relative to the cursor during placement |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DrawingFormatTitleBuilderTitleBlockPositionType Enumeration | Represent the option of TitleBlockPosition that specifies Type display |
Property Detail¶
Automatic¶
-
DrawingFormatTitleBuilder.
Automatic
¶ Returns or sets the flag that determines whether or not the title block updates automatically whenever a change occurs to a referenced object in the model
-------------------------------------
Getter Method
Signature
Automatic()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Automatic(automatic)
Parameters: automatic (bool) – New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
TitleBlockAlignmentPosition¶
-
DrawingFormatTitleBuilder.
TitleBlockAlignmentPosition
¶ Returns or sets the option that specifies how the title block aligns relative to the cursor during placement
-------------------------------------
Getter Method
Signature
TitleBlockAlignmentPosition()
Returns: Return type: NXOpen.Annotations.DrawingFormatTitleBuilderTitleBlockPositionType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TitleBlockAlignmentPosition(titleBlockAlignmentPosition)
Parameters: titleBlockAlignmentPosition ( NXOpen.Annotations.DrawingFormatTitleBuilderTitleBlockPositionType
) –New in version NX9.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
DrawingFormatTitleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.