DraftingNoteBuilderThicknessTypes Enumeration

NXOpen.Annotations.DraftingNoteBuilder.ThicknessTypes is an alias for NXOpen.Annotations.DraftingNoteBuilderThicknessTypes

class NXOpen.Annotations.DraftingNoteBuilderThicknessTypes

Bases: object

thickness types for text

Enum Members

Enum Member Enum Member Description
Medium
Medium thickness type
Thick
Thick thickness type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.