DraftingNoteBuilderTextAlign Enumeration

NXOpen.Annotations.DraftingNoteBuilder.TextAlign is an alias for NXOpen.Annotations.DraftingNoteBuilderTextAlign

class NXOpen.Annotations.DraftingNoteBuilderTextAlign

Bases: object

text over leader types for text

Enum Members

Enum Member Enum Member Description
Top
Align top
Middle
Align middle
Bottom
Align bottom
BelowbottomExtToMax
Align below bottom extension to maximum
BelowbottomExtToMaxUnderline
Align below bottom extension to maximum and underline
Belowbottom
Align below bottom
BelowbottomUnderline
Align below bottom and underline
BelowTopExtToMax
Align below top extension to maximum
BelowTopExtToMaxUnderline
Align below top extension to maximum and underline
BelowTop
Align below top
BelowTopUnderline
Align below top and underline
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.