DraftingImageFileType Enumeration

NXOpen.Annotations.DraftingImage.FileType is an alias for NXOpen.Annotations.DraftingImageFileType

class NXOpen.Annotations.DraftingImageFileType

Bases: object

The export image file types

Enum Members

Enum Member Enum Member Description
Png
PNG file type
Jpg
JPG file type
Tif
TIF file type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.