DimensionType Enumeration¶
-
class
NXOpen.Annotations.
DimensionType
¶ Bases:
object
Specifies the type of dimension being created Enum Members
Enum Member Enum Member Description AngularMajor Major Angular dimensionAngularMinor Minor Angular dimensionArcLength Arc Length dimensionBaseline Baseline dimensionChain Chain dimensionChamfer Chamfer dimensionConcentricCircle Concentric Circle dimensionCylindrical Cylindrical dimensionDiameter Diameter dimensionFoldedRadius Folded Radius dimensionHole Hole dimensionHorizontal Horizontal dimensionOrdinateHorizontal Horizontal Ordinate dimensionOrdinateOrigin Ordinate Origin dimensionOrdinateVertical Vertical Ordinate dimensionParallel Parallel dimensionPerpendicular Perpendicular dimensionRadius Radius dimensionVertical Vertical dimensionLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-