DimensionTextFormat Enumeration

class NXOpen.Annotations.DimensionTextFormat

Bases: object

Specifies the dimension text format Enum Members

Enum Member Enum Member Description
Decimal
Specifies decimal format
HalfSizeFraction
Specifies 1/2 size fraction format
TwoThirdSizeFraction
Specfies 2/3 size fraction format
FullSizeFraction
Specifies full size fraction format
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.