DimensionSetBuilder Class

class NXOpen.Annotations.DimensionSetBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.DimensionSetBuilder

This is a sub-builder class and cannot be directly instantiated

New in version NX9.0.0.

Properties

Property Description
DimensionOrSet Returns the dimension or dimension set object
Method Returns or sets the dimension set method
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

DimensionSetBuilderDimensionSetMethod Enumeration dimension set method

Property Detail

DimensionOrSet

DimensionSetBuilder.DimensionOrSet

Returns the dimension or dimension set object

-------------------------------------

Getter Method

Signature DimensionOrSet()

Returns:
Return type:NXOpen.Annotations.SelectAnnotation

New in version NX9.0.0.

License requirements: None.

Method

DimensionSetBuilder.Method

Returns or sets the dimension set method

-------------------------------------

Getter Method

Signature Method()

Returns:
Return type:NXOpen.Annotations.DimensionSetBuilderDimensionSetMethod

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Method(method)

Parameters:method (NXOpen.Annotations.DimensionSetBuilderDimensionSetMethod) –

New in version NX9.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)

Method Detail

Validate

DimensionSetBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.