DimensionMeasurementBuilderMeasurementMethod Enumeration

NXOpen.Annotations.DimensionMeasurementBuilder.MeasurementMethod is an alias for NXOpen.Annotations.DimensionMeasurementBuilderMeasurementMethod

class NXOpen.Annotations.DimensionMeasurementBuilderMeasurementMethod

Bases: object

measurement method for the dimensions

Enum Members

Enum Member Enum Member Description
Inferred
Inferred measurement direction (UI Only)
Horizontal
Horizontal measurement direction
Vertical
Vertical measurement direction
PointToPoint
Point to point measurement direction
Perpendicular
Perpendicular measurement direction
Cylindrical
Linear measurement method representing a diameter
Angular
Angular measurement type
Radial
Radial measurement type
Diametral
Diametral measurement type
HoleCallout
Hole Callout based measurement
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.