DecimalPointCharacter Enumeration

class NXOpen.Annotations.DecimalPointCharacter

Bases: object

Specifies the decimal point character Enum Members

Enum Member Enum Member Description
Period
Specifies period decimal point character
Comma
Specifies comma decimal point character
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.