DatumTargetBuilderTypes Enumeration

NXOpen.Annotations.DatumTargetBuilder.Types is an alias for NXOpen.Annotations.DatumTargetBuilderTypes

class NXOpen.Annotations.DatumTargetBuilderTypes

Bases: object

datum symbol type

Enum Members

Enum Member Enum Member Description
Point
point
Line
point
Rectangular
rectangular
Circular
circular
Annular
annular
Spherical
spherical
Cylindrical
cylindrical
Arbitrary
arbitrary
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.