DatumTargetBuilderStandardTypes Enumeration

NXOpen.Annotations.DatumTargetBuilder.StandardTypes is an alias for NXOpen.Annotations.DatumTargetBuilderStandardTypes

class NXOpen.Annotations.DatumTargetBuilderStandardTypes

Bases: object

represents the datum target standards

Enum Members

Enum Member Enum Member Description
NoStandard
NO_STANDARD
AsmeY145m1982
ASME_Y145M_1982
AsmeY145m1994
Y145M_1994
AsmeIso11011983
ISO 1101 1983
GmAddendum94
94_GM_ADDENDUM
Asig2000
ASIG_2000
AsmeY1452009
ASME_Y145_2009
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.