DatumFeatureSymbolBuilder Class

class NXOpen.Annotations.DatumFeatureSymbolBuilder

Bases: NXOpen.Builder

Represents a Base Datum Feature Symbol Builder for all types of datum feature symbols

This is an abstract class, and cannot be instantiated.

New in version NX6.0.0.

Properties

Property Description
Leader Returns the NXOpen.Annotations.LeaderBuilder for the annotation
Letter Returns or sets the datum feature string
Origin Returns the datum feature symbol origin
Style Returns the datum feature style
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
InheritFrom The datum feature symbol is inherited form the given datum feature symbol.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Leader

DatumFeatureSymbolBuilder.Leader

Returns the NXOpen.Annotations.LeaderBuilder for the annotation

-------------------------------------

Getter Method

Signature Leader()

Returns:
Return type:NXOpen.Annotations.LeaderBuilder

New in version NX6.0.0.

License requirements: None.

Letter

DatumFeatureSymbolBuilder.Letter

Returns or sets the datum feature string

-------------------------------------

Getter Method

Signature Letter()

Returns:
Return type:str

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Letter(datumFeatureLetter)

Parameters:datumFeatureLetter (str) –

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)

Origin

DatumFeatureSymbolBuilder.Origin

Returns the datum feature symbol origin

-------------------------------------

Getter Method

Signature Origin()

Returns:
Return type:NXOpen.Annotations.OriginBuilder

New in version NX6.0.0.

License requirements: None.

Style

DatumFeatureSymbolBuilder.Style

Returns the datum feature style

-------------------------------------

Getter Method

Signature Style()

Returns:
Return type:NXOpen.Annotations.StyleBuilder

New in version NX6.0.0.

License requirements: None.

Method Detail

InheritFrom

DatumFeatureSymbolBuilder.InheritFrom

The datum feature symbol is inherited form the given datum feature symbol.

Signature InheritFrom(inheritTag)

Parameters:inheritTag (NXOpen.Annotations.BaseDatum) –

New in version NX8.5.0.

License requirements: None.

Validate

DatumFeatureSymbolBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.