CuttingPlaneSymbolBuilderTextPlaneRelativeArrow Enumeration

NXOpen.Annotations.CuttingPlaneSymbolBuilder.TextPlaneRelativeArrow is an alias for NXOpen.Annotations.CuttingPlaneSymbolBuilderTextPlaneRelativeArrow

class NXOpen.Annotations.CuttingPlaneSymbolBuilderTextPlaneRelativeArrow

Bases: object

Represents position of the text relative to the arrow option

Enum Members

Enum Member Enum Member Description
Parallel
The Plane of the PMI Cutting Plane Symbol Text is Parallel to its Arrow.
Perpendicular
The Plane of the PMI Cutting Plane Symbol Text is Perpendicular to its Arrow.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.