CuttingPlaneSymbolBuilderArrowDirectionOption Enumeration¶
NXOpen.Annotations.CuttingPlaneSymbolBuilder.ArrowDirectionOption is an alias for NXOpen.Annotations.CuttingPlaneSymbolBuilderArrowDirectionOption
-
class
NXOpen.Annotations.
CuttingPlaneSymbolBuilderArrowDirectionOption
¶ Bases:
object
Represents position of the arrow direction relative to cutting plane
Enum Members
Enum Member Enum Member Description Towards The Direction of the PMI Cutting Plane Symbol Arrow Towards Plane.Away The Direction of the PMI Cutting Plane Symbol Arrow Away From Plane.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-