CommonWorkflowBuilder Class

class NXOpen.Annotations.CommonWorkflowBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.CommonWorkflowBuilder

New in version NX9.0.0.

Properties

Property Description
DynamicAlignmentInGlobalSelection Returns or sets the dynamic alignment in global selection determines whether drafting annotations and dimensions will automatically align or not when moving them in Global Selection.
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

DynamicAlignmentInGlobalSelection

CommonWorkflowBuilder.DynamicAlignmentInGlobalSelection

Returns or sets the dynamic alignment in global selection determines whether drafting annotations and dimensions will automatically align or not when moving them in Global Selection.

-------------------------------------

Getter Method

Signature DynamicAlignmentInGlobalSelection()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DynamicAlignmentInGlobalSelection(dynamicAlignmentInGlobalSelection)

Parameters:dynamicAlignmentInGlobalSelection (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

CommonWorkflowBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.