ChamferOrientationType Enumeration

class NXOpen.Annotations.ChamferOrientationType

Bases: object

Specifies the linear chamfer dimension orientation Enum Members

Enum Member Enum Member Description
Horizontal
default (same as the adjacent edge)
Vertical
perpendicular with default
Parallel
parallel to the chamfer line itself
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.