BreakSettingsBuilder Class¶
-
class
NXOpen.Annotations.
BreakSettingsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.BreakSettingsBuilder
builderNew in version NX10.0.0.
Properties¶
Property | Description |
---|---|
BreakSize | Returns or sets the break size |
CreateBreaks | Returns or sets the create breaks option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BreakSize¶
-
BreakSettingsBuilder.
BreakSize
¶ Returns or sets the break size
-------------------------------------
Getter Method
Signature
BreakSize()
Returns: Return type: float New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakSize(breakSize)
Parameters: breakSize (float) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
CreateBreaks¶
-
BreakSettingsBuilder.
CreateBreaks
¶ Returns or sets the create breaks option
-------------------------------------
Getter Method
Signature
CreateBreaks()
Returns: Return type: bool New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CreateBreaks(creatsBreak)
Parameters: creatsBreak (bool) – New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
BreakSettingsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.