BaseThicknessDimensionBuilder Class

class NXOpen.Annotations.BaseThicknessDimensionBuilder

Bases: NXOpen.Builder

Represents a NXOpen.Annotations.BaseThicknessDimensionBuilder builder

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
AppendedText Returns the appended text
FirstAssociativity Returns the first associativity
Inherit Returns the inherit
Origin Returns the origin
SecondAssociativity Returns the second associativity
Style Returns the style
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

AppendedText

BaseThicknessDimensionBuilder.AppendedText

Returns the appended text

-------------------------------------

Getter Method

Signature AppendedText()

Returns:
Return type:NXOpen.Annotations.AppendedTextBuilder

New in version NX9.0.0.

License requirements: None.

FirstAssociativity

BaseThicknessDimensionBuilder.FirstAssociativity

Returns the first associativity

-------------------------------------

Getter Method

Signature FirstAssociativity()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Inherit

BaseThicknessDimensionBuilder.Inherit

Returns the inherit

-------------------------------------

Getter Method

Signature Inherit()

Returns:
Return type:NXOpen.Annotations.SelectDimension

New in version NX9.0.0.

License requirements: None.

Origin

BaseThicknessDimensionBuilder.Origin

Returns the origin

-------------------------------------

Getter Method

Signature Origin()

Returns:
Return type:NXOpen.Annotations.OriginBuilder

New in version NX9.0.0.

License requirements: None.

SecondAssociativity

BaseThicknessDimensionBuilder.SecondAssociativity

Returns the second associativity

-------------------------------------

Getter Method

Signature SecondAssociativity()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Style

BaseThicknessDimensionBuilder.Style

Returns the style

-------------------------------------

Getter Method

Signature Style()

Returns:
Return type:NXOpen.Annotations.StyleBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

BaseThicknessDimensionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.