BaseSurfaceFinishBuilderToleranceOption Enumeration¶
NXOpen.Annotations.BaseSurfaceFinishBuilder.ToleranceOption is an alias for NXOpen.Annotations.BaseSurfaceFinishBuilderToleranceOption
-
class
NXOpen.Annotations.
BaseSurfaceFinishBuilderToleranceOption
¶ Bases:
object
the valid surface finish tolerance types
Enum Members
Enum Member Enum Member Description NotSet No toleranceEqualBilateral Equal bilateralBilateral BilateralUnilateralPlus Unilateral plusUnilateralMinus Unilateral minusPlusLimitTwoLines Plus limit two linesMinusLimitTwoLines Minus limit two linesPlusLimitOneLine Plus limit one lineMinusLimitOneLine Minus limit one line-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-