BaseRapidDimensionBuilder Class

class NXOpen.Annotations.BaseRapidDimensionBuilder

Bases: NXOpen.Builder

Represents a NXOpen.Annotations.Dimension builder

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
AppendedText Returns the appended text
FirstAssociativity Returns the first associativity
Inherit Returns the inherit
Measurement Returns the measurement
Origin Returns the origin
SecondAssociativity Returns the second associativity
Style Returns the style
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFirstAssociativityVectorFlipped First associativity vector flipped @return
GetObject Returns the object currently being edited by this builder.
GetSecondAssociativityVectorFlipped Second associativity vector flipped @return
SetFirstAssociativityVectorFlipped First associativity vector flipped
SetSecondAssociativityVectorFlipped Second associativity vector flipped
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

AppendedText

BaseRapidDimensionBuilder.AppendedText

Returns the appended text

-------------------------------------

Getter Method

Signature AppendedText()

Returns:
Return type:NXOpen.Annotations.AppendedTextBuilder

New in version NX9.0.0.

License requirements: None.

FirstAssociativity

BaseRapidDimensionBuilder.FirstAssociativity

Returns the first associativity

-------------------------------------

Getter Method

Signature FirstAssociativity()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Inherit

BaseRapidDimensionBuilder.Inherit

Returns the inherit

-------------------------------------

Getter Method

Signature Inherit()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Measurement

BaseRapidDimensionBuilder.Measurement

Returns the measurement

-------------------------------------

Getter Method

Signature Measurement()

Returns:
Return type:NXOpen.Annotations.DimensionMeasurementBuilder

New in version NX9.0.0.

License requirements: None.

Origin

BaseRapidDimensionBuilder.Origin

Returns the origin

-------------------------------------

Getter Method

Signature Origin()

Returns:
Return type:NXOpen.Annotations.OriginBuilder

New in version NX9.0.0.

License requirements: None.

SecondAssociativity

BaseRapidDimensionBuilder.SecondAssociativity

Returns the second associativity

-------------------------------------

Getter Method

Signature SecondAssociativity()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Style

BaseRapidDimensionBuilder.Style

Returns the style

-------------------------------------

Getter Method

Signature Style()

Returns:
Return type:NXOpen.Annotations.StyleBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

GetFirstAssociativityVectorFlipped

BaseRapidDimensionBuilder.GetFirstAssociativityVectorFlipped

First associativity vector flipped

Signature GetFirstAssociativityVectorFlipped()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

GetSecondAssociativityVectorFlipped

BaseRapidDimensionBuilder.GetSecondAssociativityVectorFlipped

Second associativity vector flipped

Signature GetSecondAssociativityVectorFlipped()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

SetFirstAssociativityVectorFlipped

BaseRapidDimensionBuilder.SetFirstAssociativityVectorFlipped

First associativity vector flipped

Signature SetFirstAssociativityVectorFlipped(firstVectorFlipped)

Parameters:firstVectorFlipped (bool) –

New in version NX9.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)

SetSecondAssociativityVectorFlipped

BaseRapidDimensionBuilder.SetSecondAssociativityVectorFlipped

Second associativity vector flipped

Signature SetSecondAssociativityVectorFlipped(secondVectorFlipped)

Parameters:secondVectorFlipped (bool) –

New in version NX9.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”) OR solid_modeling (“SOLIDS MODELING”)

Validate

BaseRapidDimensionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.