AssociativityPointOption Enumeration¶
-
class
NXOpen.Annotations.
AssociativityPointOption
¶ Bases:
object
Specifies the associativity point option Enum Members
Enum Member Enum Member Description NotSet No pointControl Control pointArcCenter Arc center pointTangent Tangent pointIntersection Intersection pointScreenPosition Screen positionOnCurve Point on curvePole Spline poleAnchor Conic AnchorDefining Spline defining pointLast Last enum value. Should not be used.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-