AssociativityLineOption Enumeration¶
-
class
NXOpen.Annotations.
AssociativityLineOption
¶ Bases:
object
Specifies the associativity line option Enum Members
Linear
Bolt circle
Circular
- “
- “Angle”, ” At angle ” “HorizontalRight”, ” Horizontal right ” “VerticalUp”, ” Vertical up ” “HorizontalLeft”, ” Horizontal left ” “VerticalDown”, ” Vertical down ” “BaseLine”, ” Base line ” “Last”, ” Last enum value. Should not be used. “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.