AssociativeTextPropertyType Enumeration

NXOpen.Annotations.AssociativeText.PropertyType is an alias for NXOpen.Annotations.AssociativeTextPropertyType

class NXOpen.Annotations.AssociativeTextPropertyType

Bases: object

the associative text property type to be used with the object

Enum Members

Enum Member Enum Member Description
DrawingNumberOfSheets
Drawing sheet number of sheets
DrawingNumberOfPrimarySheets
Drawing sheet number of primary sheets
DrawingSheetName
Drawing sheet name
DrawingSheetNumber
Drawing sheet number
DrawingSheetRevision
Drawing sheet revision
DrawingSheetScaleNumerator
Drawing sheet scale numerator
DrawingSheetScaleDenominator
Drawing sheet scale denominator
DrawingSheetSize
Drawing sheet size
DrawingSheetUnits
Drawing sheet units
DrawingSheetZone
Drawing sheet zone
DrawingSheetProjectionAngle
Drawing sheet projection angle
DrawingMasterPartName
Drawing master part name
DrawingPartName
Drawing part name
DrawingViewPrefix
Drawing view prefix
DrawingViewRotationAngle
View rotation angle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.