ArrowComponent Class¶
-
class
NXOpen.Annotations.
ArrowComponent
¶ Bases:
NXOpen.TransientObject
Represents a single arrow in an annotation and can be queried for information about that arrow.
This information includes the type of arrow, the origin in absolute coordinates, and the arrow angle .. versionadded:: NX6.0.2
Properties¶
Property | Description |
---|---|
ArrowAngle | Returns the arrow angle. |
IncludedArrowAngle | Returns the included arrow angle. |
Index | Returns the arrow index. |
Origin | Returns the arrow origin in absolute coordinates. |
Type | Returns the arrow type. |
Property Detail¶
ArrowAngle¶
-
ArrowComponent.
ArrowAngle
¶ Returns the arrow angle.
-------------------------------------
Getter Method
Signature
ArrowAngle()
Returns: the arrow angle Return type: float New in version NX6.0.2.
License requirements: None.
IncludedArrowAngle¶
-
ArrowComponent.
IncludedArrowAngle
¶ Returns the included arrow angle.
-------------------------------------
Getter Method
Signature
IncludedArrowAngle()
Returns: the included arrow angle Return type: float New in version NX11.0.0.
License requirements: None.
Index¶
-
ArrowComponent.
Index
¶ Returns the arrow index.
-------------------------------------
Getter Method
Signature
Index()
Returns: the arrow index Return type: int New in version NX9.0.0.
License requirements: None.
Origin¶
-
ArrowComponent.
Origin
¶ Returns the arrow origin in absolute coordinates.
If the annotation is on a drawing, origin is returned in drawing space. If the annotation is on the model, origin is returned in model space.
-------------------------------------
Getter Method
Signature
Origin()
Returns: the arrow origin in absolute coordinates Return type: NXOpen.Point3d
New in version NX6.0.2.
License requirements: None.
Type¶
-
ArrowComponent.
Type
¶ Returns the arrow type.
-------------------------------------
Getter Method
Signature
Type()
Returns: the arrow type Return type: NXOpen.Annotations.ArrowheadType
New in version NX6.0.2.
License requirements: None.
Method Detail¶
Dispose¶
-
ArrowComponent.
Dispose
¶ Free resources associated with the arrow component.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.2.
License requirements: None.