ArbitraryAreaSeedBuilder Class¶
-
class
NXOpen.Annotations.
ArbitraryAreaSeedBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.ArbitraryAreaSeedBuilder
To create a new instance of this class, use
NXOpen.Annotations.PmiManager.CreateArbitraryAreaSeedBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
SelectFace | Returns the select face |
SpecifyCurves | Returns the specify curves |
SpecifyPoint | Returns or sets the specify point |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SelectFace¶
-
ArbitraryAreaSeedBuilder.
SelectFace
¶ Returns the select face
-------------------------------------
Getter Method
Signature
SelectFace()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
License requirements: None.
SpecifyCurves¶
-
ArbitraryAreaSeedBuilder.
SpecifyCurves
¶ Returns the specify curves
-------------------------------------
Getter Method
Signature
SpecifyCurves()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
License requirements: None.
SpecifyPoint¶
-
ArbitraryAreaSeedBuilder.
SpecifyPoint
¶ Returns or sets the specify point
-------------------------------------
Getter Method
Signature
SpecifyPoint()
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpecifyPoint(specifyPoint)
Parameters: specifyPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: geometric_tol (“GDT”)
Method Detail¶
Validate¶
-
ArbitraryAreaSeedBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.