AngularDimensionFormat Enumeration

class NXOpen.Annotations.AngularDimensionFormat

Bases: object

Specifies the angular dimension format Enum Members

Enum Member Enum Member Description
FractionalDegrees
Specifies fractional degrees format
WholeDegrees
Specifies whole degrees format
DegreesMinutes
Specifies degrees minutes format
DegreesMinutesSeconds
Specifies degrees minutes seconds format
Last
Last enum value. Should not be used.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.