AlignmentPosition Enumeration¶
-
class
NXOpen.Annotations.
AlignmentPosition
¶ Bases:
object
Specifies the site location in the text box which can be used to locate a drafting object Enum Members
Enum Member Enum Member Description TopLeft TopCenter TopRight MidLeft MidCenter MidRight BottomLeft BottomCeneter Use AnnotationsAlignmentPosition.BottomCenter
insteadBottomCenter BottomRight -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-