Defun: ug_askExpressionValueAsString( Any, $expression, String, $fmt ) @{...} String;
Description: Returns the value of an expression as a string in the current Locale Type String returned Boolean TRUE or FALSE String String Number Formatted floating point %fmt Int Formatted int %fmt Vector Vector( %fmt, %fmt, %fmt ) Point Point( %fmt, %fmt, %fmt ) $fmt is the format for numeric values. For example, "%5.5f" for a number/vector/point value or "%7d" for an integer value. Input Arguments: expression - Value to get translated string from fmt - Format specifier for numeric values Returns: String- The value of the expression as a string in the current Locale See Also: