UF_UGFONT_font_header_s (view source)
Defined in: uf_ugfont.h
Also known as:
Overview
The following structure defines the font header. These are
parameters that effect all of the characters in the font.
Data Members
version
int
height
int
width
int
base_height
int
waist_height
int
width_type
int
overlap_1
int
overlap_2
int
overlap_3
int
line_spacing
double
char_spacing
double
grid_spacing
double
number_of_chars
int
identifies the format of the font binary file.
Currently this is version 1.