/*
uf_udop.h
File Description:
This is the Open C API interface to User-Defined Operations.
The user should use either an attribute (see uf_attr.h) or a User Defined
Object (see uf_udobj.h) to associate data with a User Defined Operation. If
the data is of type integer, double or string one can use either an attribute
or a User Defined Object. If the data is a link to another object and that
link must be considered for update and delete processing then a User Defined
Object is most appropriate. Attributes are simpler to use than User Defined
Objects but don't allow for automatic update and delete processing. User
Defined Objects do participate in update and delete processing.
See uf_attr.h and uf_udobj.h and the Open API User Documentation for more
information.
******************************************************************************/
#ifndef UF_UDOP_H
#define UF_UDOP_H
/***************************************************************************
***************************************************************************/
/***************************************************************************
***************************************************************************/
#include <uf_defs.h>
#include <uf_cam.h>
#include <uf_oper.h>
#include <libufun_cam_exports.h>
/********************************** Defines ***********************************/
/********************************** TypeDefs **********************************/
/* UF_UDOP_id_t is the identifier for referring to a UF_UDOP */
typedef void *UF_UDOP_id_t;
/*****************************************************************************
The following enum describes the purposes a UDO may be calling a User
Exit.
******************************************************************************/
enum UF_UDOP_purpose_e
{
UF_UDOP_USER_PARAMS, /* The user exit is being called so it can
do whatever processing it wishes to
capture the parameters for generating this
operation's toolpath.
*/
UF_UDOP_GENERATE /* The user exit is being called to generate
the tool path for this operation.
*/
};
typedef enum UF_UDOP_purpose_e UF_UDOP_purpose_t;
/****************************************************************************
NOTE :
A User Defined Operation identifier of the type UF_UDOP_id_t has to be
used as the input for all functions querying an User Defined operation
*****************************************************************************/
/******************************* Prototypes **********************************/
/*****************************************************************************
Returns the UF_UDOP_id_t that corresponds to the UF_CAM_exit_id_t passed to
the User Exit from NX.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUN_CAMEXPORT int UF_UDOP_ask_udop(
UF_CAM_exit_id_t exit_id ,/* <I>
exit_id passed to user exit from NX
*/
UF_UDOP_id_t* udop_id /* <O>
The udop of this exit_id
*/
);
/*****************************************************************************
Returns an Operation Identifier for the input UF_UDOP_id_t.
Environment: Internal and External
See Also:
History:
******************************************************************************/
extern UFUN_CAMEXPORT int UF_UDOP_ask_oper(
UF_UDOP_id_t udop_id ,/* <I>
The udop of requested oper
*/
UF_OPER_id_t* oper_id /* <O>
The oper of this udop_id
*/
);
/*****************************************************************************
Returns why the User Exit is being called. The purpose must be of type
UF_UDOP_purpose_t.
Environment: Internal and External
See Also: See UF_UDOP_purpose_t
History:
******************************************************************************/
extern UFUN_CAMEXPORT int UF_UDOP_ask_purpose(
UF_UDOP_id_t udop_id ,/* <I>
The udop of requested operation.
*/
UF_UDOP_purpose_t* purpose /* <O>
The reason the User Exit was called
*/
);
#undef EXPORTLIBRARY
#endif