/*
uf_tabnot_types.h
File Description:
This file contains the datatypes and error codes for the Tabular Note
user function module.
********************************************************************************/
#ifndef UF_TABNOT_ERRORS_H_INCLUDED
#define UF_TABNOT_ERRORS_H_INCLUDED
#include <uf_defs.h>
#define UF_TABNOT_fit_method_max UF_TABNOT_fit_method_truncate
#define UF_TABNOT_nm_fit_methods UF_TABNOT_fit_method_max
#define UF_TABNOT_APPEND (-1)
enum UF_TABNOT_header_location_t
{
UF_TABNOT_header_location_none,
UF_TABNOT_header_location_above,
UF_TABNOT_header_location_below
};
enum UF_TABNOT_overflow_direction_t
{
UF_TABNOT_overflow_left = 1,
UF_TABNOT_overflow_right,
UF_TABNOT_overflow_next_sheet
};
enum UF_TABNOT_display_continuation_note_t
{
UF_TABNOT_display_continuation_note_none,
UF_TABNOT_display_continuation_note_above,
UF_TABNOT_display_continuation_note_below
};
enum UF_TABNOT_attach_point_t
{
UF_TABNOT_attach_point_top_left = 1,
UF_TABNOT_attach_point_top_right,
UF_TABNOT_attach_point_bottom_left,
UF_TABNOT_attach_point_bottom_right
};
/* Text formats */
enum UF_TABNOT_format_t
{
UF_TABNOT_format_text = 1,
UF_TABNOT_format_float,
UF_TABNOT_format_fixed,
UF_TABNOT_format_general,
UF_TABNOT_format_monetary,
UF_TABNOT_format_comma,
UF_TABNOT_format_fraction_half_size,
UF_TABNOT_format_fraction_three_quarter_size,
UF_TABNOT_format_fraction_full_size,
UF_TABNOT_format_percent,
UF_TABNOT_format_degrees,
UF_TABNOT_format_degrees_radian_units,
UF_TABNOT_format_degrees_degree_units,
UF_TABNOT_format_hex,
UF_TABNOT_format_logic,
UF_TABNOT_format_date_dmy,
UF_TABNOT_format_date_dm,
UF_TABNOT_format_date_my,
UF_TABNOT_format_date_mdy,
UF_TABNOT_format_date_ymd,
UF_TABNOT_format_date_y4md,
UF_TABNOT_format_date_dmy_dot,
UF_TABNOT_format_time_hm,
UF_TABNOT_format_time_hms,
UF_TABNOT_format_hidden,
UF_TABNOT_format_custom
};
/* Determines how to display a single 0 */
enum UF_TABNOT_zero_display_t
{
UF_TABNOT_zero_display_zero,
UF_TABNOT_zero_display_dash,
UF_TABNOT_zero_display_empty
};
/* Text justification values */
enum UF_TABNOT_just_t
{
UF_TABNOT_just_left,
UF_TABNOT_just_center,
UF_TABNOT_just_right,
UF_TABNOT_just_top = 0,
UF_TABNOT_just_middle,
UF_TABNOT_just_bottom
};
/* Method used to fit text within a cell. If
no methods are specified, the fallback
method is error display (########). */
enum UF_TABNOT_fit_method_t
{
UF_TABNOT_fit_method_none,
UF_TABNOT_fit_method_overwrite_border,
UF_TABNOT_fit_method_auto_size_text,
UF_TABNOT_fit_method_wrap,
UF_TABNOT_fit_method_abbreviate,
UF_TABNOT_fit_method_remove_spaces,
UF_TABNOT_fit_method_auto_size_row,
UF_TABNOT_fit_method_auto_size_col,
UF_TABNOT_fit_method_truncate
};
/* Sort direction */
enum UF_TABNOT_sort_direction_t
{
UF_TABNOT_sort_dir_descending=0,
UF_TABNOT_sort_dir_ascending
};
struct UF_TABNOT_section_prefs_s
{
UF_TABNOT_header_location_t header_location; /* Location to display header */
double max_height; /* The maximum height of the
section. This will determine
the number of rows contained in
the section. */
UF_TABNOT_overflow_direction_t overflow_direction; /* Direction to overflow sections */
double overflow_spacing; /* Distance to offset continuation
sections (only used when table
continues on the same sheet) */
UF_TABNOT_attach_point_t attach_point; /* Point to which origin is attached */
logical use_double_width_border; /* Should the border be double width? */
double border_width; /* Width of border if use_double_width_border
is TRUE */
UF_TABNOT_display_continuation_note_t display_continuation_note; /* Display continuation note flag<DRF30825> */
char* continuation_note; /* Continuation note string */
};
typedef struct UF_TABNOT_section_prefs_s UF_TABNOT_section_prefs_t, *UF_TABNOT_section_prefs_p_t;
struct UF_TABNOT_cell_prefs_s
{
UF_TABNOT_format_t format; /* Cell format */
int precision; /* Precision (# dec places to the
right of the decimal point) */
logical is_a_formula; /* Does the formatted text get
passed to the expression
subsystem for evaluation */
UF_TABNOT_zero_display_t zero_display; /* The way that a numeric zero
should display */
int text_font; /* Index of NX font */
double text_height; /* Height of text in this cell */
double text_aspect_ratio; /* Text aspect ratio */
UF_TABNOT_just_t horiz_just; /* Horizontal text justification */
UF_TABNOT_just_t vert_just; /* Vertical text justification */
double text_angle; /* Text angle in radians */
double text_slant; /* Text slant angle */
logical is_vertical; /* Is text displayed vertical? */
logical is_italic; /* Is text displayed italic? */
logical strikethru; /* Is text stricken thru? */
double line_space_factor; /* Line space factor */
double char_space_factor; /* Character space factor */
logical is_hidden; /* Is display of text suppressed? */
int text_color; /* Text color */
int text_density; /* Text density 1:Normal, 2:Heavy, 3:Thin, 0:Use Default*/
int bottom_line_cfw[3]; /* Color/font/width of bottom line */
int right_line_cfw[3]; /* Color/font/width of right line
width follows 1:Normal, 2:Heavy, 3:Thin, 0:Use Default*/
int nm_fit_methods; /* Number of fit methods */
UF_TABNOT_fit_method_t fit_methods[UF_TABNOT_fit_method_max]; /* Fit methods */
tag_t referenced_spreadsheet; /* Referenced spreadsheet */
int ss_sheet; /* Sheet referenced in spreadsheet */
int ss_row; /* Row referenced in spreadsheet */
int ss_col; /* Column referenced in spreadsheet */
char* prefix;
char* suffix;
char* formula_suffix; /* This string gets appended to the
cell text when the text is passed
to the expression subsystem when
evaluating the cell as a formula. */
char* url;
logical is_protected; /* Is cell protected? */
};
typedef struct UF_TABNOT_cell_prefs_s UF_TABNOT_cell_prefs_t, *UF_TABNOT_cell_prefs_p_t;
struct UF_TABNOT_sort_data_s
{
int sort_index; /* Index used to indicate the
order of precedence one
column has over another
when sorting the rows.
Sorting occurs first using
the column with a sort_index
of 1, then on the column
with a sort_index of 2 and
so on. A value of 0 means
"do not sort on this column".*/
UF_TABNOT_sort_direction_t sort_direction; /* Direction of the sort */
};
typedef struct UF_TABNOT_sort_data_s UF_TABNOT_sort_data_t, *UF_TABNOT_sort_data_p_t;
#define ERROR_UF_TABNOT_base 3500000
#define UF_TABNOT_ERROR_BASE ERROR_UF_TABNOT_base
#define UF_TABNOT_ERROR_RANGE 5000
#define UF_TABNOT_NO_ERRORS 0
#define UF_TABNOT_invalid_header_location (ERROR_UF_TABNOT_base + 1)
#define UF_TABNOT_invalid_overflow_direction (ERROR_UF_TABNOT_base + 2)
#define UF_TABNOT_invalid_attach_point (ERROR_UF_TABNOT_base + 3)
#define UF_TABNOT_invalid_text_format (ERROR_UF_TABNOT_base + 4)
#define UF_TABNOT_invalid_zero_display (ERROR_UF_TABNOT_base + 5)
#define UF_TABNOT_invalid_text_justification (ERROR_UF_TABNOT_base + 6)
#define UF_TABNOT_invalid_fit_method (ERROR_UF_TABNOT_base + 7)
#define UF_TABNOT_invalid_precision (ERROR_UF_TABNOT_base + 8)
#define UF_TABNOT_invalid_text_height (ERROR_UF_TABNOT_base + 9)
#define UF_TABNOT_invalid_text_aspect_ratio (ERROR_UF_TABNOT_base + 10)
#define UF_TABNOT_invalid_text_line_space_factor (ERROR_UF_TABNOT_base + 11)
#define UF_TABNOT_invalid_text_char_space_factor (ERROR_UF_TABNOT_base + 12)
#define UF_TABNOT_invalid_density (ERROR_UF_TABNOT_base + 13)
#define UF_TABNOT_invalid_tabnot_tag (ERROR_UF_TABNOT_base + 14)
#define UF_TABNOT_invalid_section_tag (ERROR_UF_TABNOT_base + 15)
#define UF_TABNOT_invalid_row_tag (ERROR_UF_TABNOT_base + 16)
#define UF_TABNOT_invalid_col_tag (ERROR_UF_TABNOT_base + 17)
#define UF_TABNOT_invalid_cell_tag (ERROR_UF_TABNOT_base + 18)
#define UF_TABNOT_invalid_plist_tag (ERROR_UF_TABNOT_base + 19)
#define UF_TABNOT_invalid_plist_row_tag (ERROR_UF_TABNOT_base + 20)
#define UF_TABNOT_invalid_plist_col_tag (ERROR_UF_TABNOT_base + 21)
#define UF_TABNOT_invalid_template_file_name (ERROR_UF_TABNOT_base + 22)
#define UF_TABNOT_invalid_display_continuation_note (ERROR_UF_TABNOT_base + 23)
/* error 300-500 reserved for hole table */
#define UF_HOLETABLE_invalid_selection (UF_TABNOT_ERROR_BASE + 301)
#define UF_HOLETABLE_view_already_selected (UF_TABNOT_ERROR_BASE + 302)
#define UF_HOLETABLE_invalid_input (UF_TABNOT_ERROR_BASE + 303)
#define UF_HOLETABLE_TABNOT_NO_ERRORS (UF_TABNOT_ERROR_BASE + 304)
#define UF_HOLETABLE_TABNOT_internal_error (UF_TABNOT_ERROR_BASE + 305)
#define UF_HOLETABLE_invalid_ordinate_origin (UF_TABNOT_ERROR_BASE + 306)
#define UF_HOLETABLE_invalid_selected_object (UF_TABNOT_ERROR_BASE + 307)
#define UF_HOLETABLE_IGNORED_HOLE (UF_TABNOT_ERROR_BASE + 308)
/* error 501-700 reserved for bend table */
#define UF_BENDTABLE_zero_columns_error (UF_TABNOT_ERROR_BASE + 501)
#endif /* UF_TABNOT_ERRORS_H_INCLUDED */