Optional SO second direction to apply to the steep faces from the first direction. This must not be parallel with the first direction. It applies a second isocline direction to the resultant steep faces from the first direction using the same angle expression. If this option is used, the angle expression must be positive.