UF_STUDIO_stybld_data_s (view source)
Defined in: uf_studio.h
Also known as:
- UF_STUDIO_stybld_data_t
- UF_STUDIO_stybld_data_p_t
Overview
Data structure for styled blend creation and editing.
Data Members
method
num_faces1
int
faces1
reverse_normal1
num_faces2
int
faces2
reverse_normal2
floating_mode
edge_1
edge_2
trim_1
double
trim_2
double
continuity_blend_1
continuity_blend_2
spine
profile_curve
depth
skew
distance_tol
double
angle_tol
double
reverse_direction1
reverse_direction2
continuity1
continuity2
direction1
direction2
stiffness
trim
curve1
curve2
curve_trans1
curve_trans2
center_curve
reverse_center_curve
center_as_spine
int
start_extension
double
end_extension
double
min_radius_mode
min_radius
char *
v_degree