UF_SKET_assoc_mod_e (view source)
Defined in: uf_sket_types.h
Also known as:
Data Members
UF_SKET_first_end_point
UF_SKET_last_end_point
UF_SKET_assoc_type_e (view source)
Defined in: uf_sket_types.h
Also known as:
Overview
Associativity types for sketch dimension.
Data Members
UF_SKET_assoc_type_none
UF_SKET_end_point
UF_SKET_arc_center
UF_SKET_tangency
UF_SKET_curve_point
UF_SKET_anchor_point
UF_SKET_con_class_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_con_class_t
- UF_SKET_con_class_p_t
Data Members
UF_SKET_no_cons
UF_SKET_all_cons
UF_SKET_geo_cons
UF_SKET_dim_cons
UF_SKET_con_type_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_con_type_t
- UF_SKET_con_type_p_t
Data Members
UF_SKET_no_con
UF_SKET_fixed
UF_SKET_horizontal
UF_SKET_vertical
UF_SKET_parallel
UF_SKET_perpendicular
UF_SKET_collinear
UF_SKET_equal_length
UF_SKET_equal_radius
UF_SKET_constant_length
UF_SKET_constant_angle
UF_SKET_coincident
UF_SKET_concentric
UF_SKET_mirror
UF_SKET_point_on_curve
UF_SKET_midpoint
UF_SKET_tangent
UF_SKET_radius_dim
UF_SKET_diameter_dim
UF_SKET_horizontal_dim
UF_SKET_vertical_dim
UF_SKET_parallel_dim
UF_SKET_perpendicular_dim
UF_SKET_angular_dim
UF_SKET_reserved_con_1
UF_SKET_reserved_con_2
UF_SKET_reserved_con_3
UF_SKET_reserved_con_4
UF_SKET_reserved_con_5
UF_SKET_reserved_con_6
UF_SKET_point_on_string
UF_SKET_slope
UF_SKET_uniform_scaled
UF_SKET_non_uniform_scaled
UF_SKET_assoc_trim
UF_SKET_assoc_offset
UF_SKET_perimeter_dim
UF_SKET_pgm_offset
UF_SKET_normal
UF_SKET_point_on_loop
UF_SKET_recipe_trim
UF_SKET_pattern
UF_SKET_rigid_set
UF_SKET_g1
UF_SKET_g2
UF_SKET_last_con_type
UF_SKET_geom_vertex_e (view source)
Defined in: uf_sket_types.h
Also known as:
Overview
enum and structures for createing geometric constraints
Data Members
UF_SKET_no_vertex
UF_SKET_start_vertex
UF_SKET_end_vertex
UF_SKET_center_vertex
UF_SKET_spline_defining_point
UF_SKET_anchor_vertex
UF_SKET_spline_pole
UF_SKET_help_type_e (view source)
Defined in: uf_sket_types.h
Also known as:
Data Members
UF_SKET_no_help_data
UF_SKET_use_help_pt
UF_SKET_use_help_param
UF_SKET_reference_status_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_reference_status_t
Data Members
UF_SKET_reference
UF_SKET_active
UF_SKET_status_e (view source)
Defined in: uf_sket_types.h
Also known as:
- UF_SKET_status_t
- UF_SKET_status_p_t
Overview
As of V17, the values of these UF_SKET_status_e will be recorded in
the part file. Hence, their values cannot be arbitrarily changed.
Data Members
UF_SKET_unknown_status
UF_SKET_not_evaluated
UF_SKET_under_constrained
UF_SKET_well_constrained
UF_SKET_over_constrained
UF_SKET_inconsistently_constrained