UF_SF_ugs_tet_mesh_parms_s (view source)
Defined in: uf_sf_ugs_mesh.h
Also known as:
- UF_SF_ugs_tet_mesh_parms_t
- UF_SF_ugs_tet_mesh_parms_p_t
Overview
Structure :- UF_SF_ugs_tet_mesh_parms_s
This structure allows specification of tetrahedral meshing parameters.
Initialization :- This structure can be initialized with the
UF_SF_ugs_tet_mesh_parms_INIT macro.
Data Members
element_type
midnodes
int
element_size
double
midnode_option
maximum_midnode_jacobian
double
minimum_face_angle
double
surf_mesh_size_variation
int
tet_mesh_size_variation
int
mesh_transition
int
remesh_toggle
int
create_pyramids
int
small_feature
double
attempt_mapped_meshing
int
two_element_through_thickness_toggle
int
auto_fix_failed_elements_toggle
int
edge_merge_toggle
int
edge_angle
double
fillet_toggle
int
fillet_type
fillet_num_elem
int
fillet_min_rad
double
fillet_max_rad
double