Distance tolerance value used to find the matched edges. The distance is measured from the mid point location of one edge to the mid point of the other edge. The default value is 0.02.
node_uniq_tol
double
Specifies the maximum distance allowed between nodes before they are merged when uniqueness testing is active. The default is 0.0001.
smooth_tol
double
Distance in model units from old position to new position for the node moved the farthest during one iteration of the smoothing algorithm. The default value is 0.01.
on_surf_tol
double
Controls the maximum distance in model units that a node created during Scenario Shell Mesher may lie from its closest point on the surface. The default value is 0.001.
trans_rows
int
Allows to control the number of rows that will be used to bridge the gap between elements of different sizes. The default value is 3.
matched edges. The distance is measured from
the mid point location of one edge to the mid
point of the other edge. The default value
is 0.02.