UF_SF_section_src_properties_s (view source)
Defined in: uf_sf_types.h
Also known as:
- UF_SF_section_src_properties_t
- UF_SF_section_src_properties_p_t
Overview
Stress recovery locations of 1D Element Sections.
First are the numeric values, followed by corresponding expressions
tags, when any location has an expression.
If there is no expression, then the tag is NULL_TAG.
Data Members
C1
double
C2
double
D1
double
D2
double
E1
double
E2
double
F1
double
F2
double
C1_exp
C2_exp
D1_exp
D2_exp
E1_exp
E2_exp
F1_exp
F2_exp