UF_SF__orthotropic_s (view source)
Defined in: uf_sf_types.h
Also known as:
Data Members
youngs_modulus [ 3 ]
poissons_ratio [ 3 ]
mass_density
shear_modulus [ 3 ]
thermal_coeff [ 3 ]
reference_temperature
thermal_conduct [ 3 ]
specific_heat
latent_heat
phase_temperature
phase_temperature_range
phase_specific_heat
ir_scattering_coeff
solar_scattering_coeff
ir_extinction_coeff
solar_extinction_coeff
electrical_resistivity
max_stress_tension [ 3 ]
max_stress_compression [ 3 ]
max_in_plane_shear_stress
max_strain_tension [ 3 ]
max_strain_compression [ 3 ]
max_in_plane_shear_strain
tsai_wu_interaction
damping_coeff