This field is set to one or more of the following symbols OR'd together to indicate which of the remaining fields of the structure are set. UF_LEGEND_WIDTH_ATTR UF_LEGEND_BORDER_ATTR UF_LEGEND_FONT_SIZE_ATTR UF_LEGEND_HEADER_ATTR UF_LEGEND_INDEX_ATTR UF_LEGEND_FOOTER_ATTR
width_percent
int
The percentage of the display which the legend occupies. The legend takes up the full height of the display. default: 20%
Switch indicating whether or not the border of the legend gets displayed. = TRUE -> display border = FALSE -> do not display border. (default)
font_size
double
The size in inches of an individual character. If not specified, the font is automatically calculated so that 15 characters can be displayed in the full width of the legend. The auto size also is constrained by a maximum size of .12" and a minimum size of .04". default: automatic
symbols OR'd together to indicate which of the
remaining fields of the structure are set.
UF_LEGEND_WIDTH_ATTR
UF_LEGEND_BORDER_ATTR
UF_LEGEND_FONT_SIZE_ATTR
UF_LEGEND_HEADER_ATTR
UF_LEGEND_INDEX_ATTR
UF_LEGEND_FOOTER_ATTR