/*
uf_route_ugopenint.h
File description:
Open C API interface to the Routing (ROUTE) module.
Please refer to uf_route.h's documentation for a discussion of Concepts
and Terminology.
******************************************************************************/
#ifndef UF_ROUTE_UGOPENINT_H_INCLUDED
#define UF_ROUTE_UGOPENINT_H_INCLUDED
/**************
** Includes **
**************/
#include <libugopenint_exports.h>
/*********************************************************************
** Function Prototypes **
********************************************************************/
/* Custom Routing Applications */
/**********************************************************************
Registers a Routing custom application. This routine should be
called just after UF_MB_register_application().
Environment: Internal
See Also:
Please refer to the example
History: Original release was in V14.0.
**********************************************************************/
extern UGOPENINTEXPORT int UF_ROUTE_register_custom_app(
int app_id /* <I>
Application ID for this application. This is returned
from UF_MB_register_application.
*/
);
/**********************************************************************
Enters a custom Routing application.
Environment: Internal
See Also:
Please refer to the example
History: Original release was in V14.0.
**********************************************************************/
extern UGOPENINTEXPORT int UF_ROUTE_enter_custom_app( void );
/**********************************************************************
Initializes a Routing custom application.
Environment: Internal
See Also:
Please refer to the example
History: Original release was in V14.0.
***********************************************************************/
extern UGOPENINTEXPORT int UF_ROUTE_init_custom_app( void );
/**********************************************************************
Exits a custom Routing application.
Environment: Internal
See Also:
Please refer to the example
History: Original release was in V14.0.
***********************************************************************/
extern UGOPENINTEXPORT int UF_ROUTE_exit_custom_app( void );
#undef EXPORTLIBRARY
#endif /* UF_ROUTE_UGOPENINT_H_INCLUDED */