UF_PATH_rotate_s
(view source)
Defined in: uf_path.h
Also known as:
UF_PATH_rotate_t
Overview
Specify data for the ROTATE/ post command.
Data Members
rotation_angle
double
is the angle by which
to rotate.
rotation_object
UF_PATH_rotation_object_t
rotation_type
UF_PATH_rotation_type_t
rotation_direction
UF_PATH_direction_t
angle_flag
logical
the rotation angle is
output if and only if
this flag is TRUE.
rotref_flag
logical
the string ROTREF is
output if and only if this
flag is TRUE.
to rotate.